Hilti
Hilti Canada
(800) 363-4458
| EN | FR

Go

The New HIT-RE 500


When a fastening system has to be specified, reliability in very diverse conditions is a key criterion for the specifier. The new adhesive in the well proven Hilti HIT foil pack is exceptionally insensitive to oversized or wet anchor holes, and it doesn't matter whether they were drilled with a rotary hammer or diamond coring machine.

Users want sufficient time to install very long rebar, but also an adhesive that cures within a practical time. Hilti-HIT RE 500 optimally meets these apparently contradictory requirements.

The new Hilti HIT-RE 500 epoxy system leaves nothing to chance. At room temperature the high-strength formula of the RE 500 allows a generous working time of approximately 30 minutes and an approximate cure time of only 12 hours. Both the working and cure times of this innovative anchoring system beat similar anchoring systems hands down. In addition, the reliable RE 500 was designed for a temperature range from 23° F (-5° C) to 104° F (40° C) and can withstand harsh temperatures making it an epoxy for all seasons.

Exclusive to Hilti, the RE 500 is red in color to help ensure accurate jobsite inspections. This and other qualities make the RE 500 the anchoring adhesive of choice. The RE 500 will stand up to even the most challenging installations and will help save time and labor on the project.
Visit the HIT RE 500 catalog page