Hilti
Hilti Canada
(800) 363-4458
| EN | FR

Go

Corrosion


Anchor Specifier Area: Corrosion
Contents
- The Corrosion Process
- Direct Chemical Attack
- Electro-Chemical Corrosion
- Corrosion Protection
- Hilti Anchors
- Organic Coatings

1 The Corrosion Process
In broad terms corrosion has been defined as the destructive alteration of a substance (usually a metal) because of a reaction with its environment. The corrosion process is very complex and has many aspects, all of which lead to the same destructive result. In the design of anchors and fasteners the most common types of corrosion are direct chemical attack and electrochemical reaction.

2 Direct Chemical Attack
Corrosion by direct chemical attack occurs when the base material is soluble in the corroding medium. One solution for this type of corrosion is to select an anchor or fastener material which is not susceptible to attack by the corroding chemical. Many books present compatibility tables which provide a guide for selecting the proper materials.

When selecting a base metal which is compatible with the corroding medium is not possible or economical, another solution is to provide a coating which is impervious to the corroding medium. These might include metallic coatings such as zinc or cadmium or organic coatings such as epoxies or fluorocarbons.

3 Electro-Chemical Corrosion
All metals have an electrical potential relative to each other and have been ranked, accordingly, to form the "electromotive force series" or "galvanic series" of metals. When metals of different potential contact in the presence of an electrolyte, the more active metal (more negative potential) becomes the anode and corrodes, while the other metal becomes the cathode and is galvanically protected.

The severity and rate of attack will be influenced by the relative position of the contacting metals in the galvanic series, the relative area of the contacting metals, and the conductivity of the electrolyte.

For anchoring and fastening applications, galvanic corrosion can be reduced by:

  1. Using similar metals or metals close together in the electromotive force series;
  2. Separating dissimilar metals with non-conductive gaskets, plastic washers or paint;
  3. Selecting materials so that the anchor or fastener is the cathode;
  4. Providing drainage to prevent entrapment of the electrolyte.

4 Corrosion Protection
The most common type of corrosion protection for carbon steel fasteners and anchors is zinc. Zinc coatings can be uniformly applied by a variety of methods to achieve a wide range of coating thicknesses. As a rule, thicker coatings provide a higher level of protection.

Based on research by ASTM and other organizations the estimated mean corrosion rate for zinc coatings in various atmospheres is shown in the table. These values are for reference only, due to the large variances in the research findings.

Zinc coatings can be applied to anchors and fasteners by different methods. Applicable ASTM specifications are as follows:

Galvanic Series of Metals and Alloys
Corroded End (anodic,or least noble)
Magnesium
Magnesium alloys
Zinc
Aluminum 1100
Cadmium
Aluminum 2024-T4
Steel or Iron
Cast Iron
Chromium-iron (active)
Ni-Resist cast iron
Type 304 Stainless (active)
Type 316 Stainless (active)
Lead tin solders
Lead
Tin
Nickel (active)
Inconel nickel-chromium alloy (active)
Hastelloy Alloy C (active)
Brasses
Bronzes
Monel nickel-copper alloy
Copper
Copper-nickel alloys
Silver solder
Nickel (passive)
Inconel nickel-chromium alloy (passive)
Chromium-iron (passive)
Type 304 Stainless (passive)
Type 316 Stainless (passive)
Hastelloy Alloy C (passive)
Silver
Titanium
Platinum
Graphite
Gold
Protected End (cathodic,or most noble)

AtmosphereMean Corrosion Rate
Industrial5.6 µm/year
Urban Non-Industrial or Marine1.5 µm/year
Suburban1.3 µm/year
Rural0.8 µm/year
IndoorsConsiderably less than 0.5 µm/year

5 Hilti Anchors
Most Hilti metal anchors are available in carbon steel with an electrodeposited zinc coating of at least 5 µm with chromate passivation.

Hilti standard and super HAS threaded rods in 7/8" diameter size are zinc coated to at least 45 µm by the hot-dip process for use on highway applications.

Where the long-term integrity of a fastening is important, and there is risk of corrosion of a carbon steel anchor, then stainless steel should be specified. Under certain conditions, even stainless steel anchors will corrode and a suitable protective coating should be specified by the designer.

It is not feasible to hot-dip galvanize expansion anchors. Zinc is relatively soft, and thick coatings tend to act as a lubricant to reduce the anchor tension capacity.

Suggested protection against corrosion
Protection against corrosionConditions of Use
Galvanic zinc plating 5-10 µm
  ASTM B633, Type III,SC1
-Inside rooms without any particular influence of moisture; or
- If covered sufficiently by concrete
Hot-dip galvanizing >= 45 µm
  ASTM A153
- Inside applications in damp rooms and near the sea
- Outside applications in only slightly corrosive country atmosphere
Stainless steel*
  AISI 303
  AISI 304
-Inside applications where there is heavy condensation
-Outside applications in corrosive atmosphere
  AISI 316** 
*Austenitic CrNi Steel
**Use of 316 stainless steel in environments where pitting or stress corrosion is likely (i.e. chlorides and water mixtures) should be avoided due to the possibility of sudden failure without visual warning.

6 Organic Coatings
Hilti Kwik-Cote is a unique organic coating which helps protect against galvanic corrosion. Hilti provides the Kwik-Cote organic coating on Kwik-Pro self drilling screws.

Return to Top